cancel
Showing results for 
Search instead for 
Did you mean: 

RLink question

lseletron
Associate II
Posted on August 30, 2007 at 22:12

RLink question

1 REPLY 1
lseletron
Associate II
Posted on August 30, 2007 at 22:12

Hi,

To program my hardware (a small device) I use ICC and ST7MDT10-EPB and everything works OK.

I bought recently an RLink and after having installed all drivers, I tried to program the same hardware but it did not work. STVD7 says ''Check pins connectors etc''.

While experimenting I might have plugged the RLink ICC connector the other way round into the hardware's ICC header.

Is it possible that the RLink is destroyed?

How can I test that it is working?

Without connecting to the hardware I can see a pulse on pin 8