2006-02-09 12:14 AM
SofTec inDART-STX/D and 12v on Vpp/ICCSEL
2006-02-08 10:25 PM
Hello.
I am going to write IAP bootloader. To erase/write flash i need 12v on Vpp/ICCSEL pin. By the way i use SofTec inDART-STX/D that uses the same pin for its own purposes. As i determined, debugger puts 12v on this pin during erase/write at the beggining of debug session. I am not so crazy 🙂 to develop bootloader without debuger. Is there any possibilities to have both debugger and 12v and not to damage debugger? The easiest way is to use switch to connect/disconnect debugger and 12v. Any another ideas?2006-02-08 11:54 PM
What about to use Schotky Diode in between your application and InDART?
Maybe BAR43C could be nice, dual schotky in one package - one for InDART, one for your application....'?2006-02-09 12:14 AM
Easy solution :-]
Tnx a lot.