2006-02-07 11:12 PM
2005-07-22 04:34 AM
I'm trying to implement a skip-jump table for my IAP project but have not yet figured out how to write a function call (using C with Cosmic compiler) at a specific location in memory. For example, how do I write a function CALL at location 0xDFDC in memory.
I've already have the vector table (in sector 0) loaded with the correct addresses of where the function CALLS should be (in sector 2). I just don't know how to write those function calls. AN1796 shows example of skip-jump table written in assembly, which is fine. But what they have doesn't work using the Cosmic compiler. This is what they have: Here's a snipit of the code example: segment byte at: FDD0 'program' jp dummyisr This appears to be exactly what I need, however, the ''segment byte at:'' command, which I assume forces the ''jp dummyisr'' command at that specific location (0xFDD0), is not recognized by Cosmic compiler. How do I effectively do the same type of thing with Cosmic. Also, is there a way to do this in C? I thought the ''@ 0xFDDC'' would somehow work, but am having no luck. Hope someone can shed some light! 🙂2005-07-24 10:59 PM
There are two ways in C language to declaire a pointer to a function/procedure. With these pointers you can form a jump-table as you do it in the vectortable.
I give you an example: - 1st declaration: void (* const proc1[3])(void) = { Task_1, /* Task_1() to Task_3() are ... */ Task_2, /* ...void procedures, already declared anywhere before */ Task_3 }; - 2nd via typedef (already predefined in the systemheader stdtypes.h of the HiWare Compiler. Don't know how Cosmic does it.): ... typedef void (*PROC)(void); /* parameterless function pointer (Procedure variable) */ ..... const PROC proc2[3] = { Task_1, Task_2, Task_3 }; const PROC proc3 = Task_1; /* single pointer */ .... And you call the procedures of your table with ..... proc1[0](); proc1[1](); proc1[2](); proc2[0](); proc2[1](); proc2[2](); ..... or the single one .... proc3(); .... Best regards WoRo2005-07-25 09:43 PM
Scooby,
please find below one possible way of addressing you problem (redirecting interrupt vectors for use with IAP). It contains some inline assembler but I think it's more clear this way (I can give you a full C solution if needed). Hope it helps. Regards, Luca (Cosmic) ***************************************** try the following: your vector table (file vector.c) extern char INT_jump_table[]; char * const _vectab[] = { INT_jump_table, INT_jump_table + 3, INT_jump_table + 6, }; and the corresponding line in the linker file +seg .const -b 0xffe0 # vectors start address vector.o your actual vectors should be defined as follows: #pragma section(INT_JMP) char INT_jump_table() { #asm xref _irq_trap,_irq_sci,_irq_rtc; jp _irq_trap // PWM ART jp _irq_sci // SCI jp _irq_rtc // MCC/RTC #endasm } #pragma END and the section placed in the linker file as +seg .INT_JMP -b 0x1000 I've tried on my PC and it works as I think you expect; the vector addresses will be ffe0 1000 bset ffe2 1003 bset ffe4 1006 bset and at address 0x1000 you will find 1000 ccfaf7 jp _irq_trap 1003 ccfaf8 jp _irq_sci 1006 ccfaf9 jp _irq_rtc Regards, Luca2006-01-02 07:52 PM
Quote:
On 26-07-2005 at 10:13, Anonymous wrote: Scooby, please find below one possible way of addressing you problem (redirecting interrupt vectors for use with IAP). It contains some inline assembler but I think it's more clear this way (I can give you a full C solution if needed). Hope it helps. Regards, Luca (Cosmic) ***************************************** Hi Luca ! Can you send me please C solution of redirecting interrupt vectors for use with IAP ? my email: sergey@sysmop.com Best regards !2006-02-07 12:08 AM
Hello, _luca.
Could you provide me with code as well. I will be much appreciated. my mail is :mailto:andrei.kirys@erl-elektronik.de
Tnx.2006-02-07 11:06 PM
Hi,
I'm afraid I have been a bit optimistic when talking about a ''full C solution''... With reference to the original solution proposed above: - the declaration of the jump table can only be done in assembler; I know no ways of having the compiler generate a list of jumps like that. - the declaration of the vectors can be done in a different way, maybe more portable, but also less readable, in my opinionCode:
typedef struct jump { // the typedef eases the next constructs char jmp_code; void (*addr); } JUMP; JUMP jump_table[10] @0x1000; // with the actual number of vectors JUMP * const vectab[] = { // this is the processor vector table &jump_table[0], &jump_table[1], &jump_table[2], }; will generate the same code (actually, only a set of addresses) as the originally proposedCode:
extern char INT_jump_table[]; char * const _vectab[] = { INT_jump_table, INT_jump_table + 3, INT_jump_table + 6, }; hope it helps. Regards, Luca (Cosmic)2006-02-07 11:12 PM
Tnx for help.