cancel
Showing results for 
Search instead for 
Did you mean: 

BOOT PIN,S Setting ???????

zero-bit
Associate
Posted on June 17, 2005 at 07:08

BOOT PIN,S Setting ???????

1 REPLY 1
zero-bit
Associate
Posted on June 16, 2005 at 11:07

BOOTEN BOOT0 BOOT 1 MEMORY

0 X X FLASH (Internal)

1 0 0 FLASH (Internal)

1 1 0 RAM (Internal)

1 0 1 System-Memory

1 1 1 External Memory Bank 0(CS0 AREA : 0x60000000H)

1) When booting with boot option which is set 1 1 1 according to above, which is prior, CS0 signal or execution of StartupCODE?

2) In JTAGE DEBUGING MODE, should RAM(Internal) be set to 1 1 0?

Now debugging is possible although composition of hardware is set to 1 1 1(External flash).

3) Must V18 Voltage be supplied from external?

*** My Configreation

CPU : STR710FZ

ADS/AXD/MultiICE

[ This message was edited by: Number2 on 16-06-2005 14:53 ]