cancel
Showing results for 
Search instead for 
Did you mean: 

Distance with ST7538

info79
Associate II
Posted on April 23, 2007 at 09:19

Distance with ST7538

6 REPLIES 6
info79
Associate II
Posted on June 27, 2005 at 13:42

I'm tryng to develop a system based on ST7538. I'm in trouble with distance between master station and slave.

a) Is there any way to simulate distance in power line ?

b) Which the problems in power lines ?

c) Shall I comunicate over 1 Km with power line ?

Thanks for your Help,

Best Regards,

franco
Associate II
Posted on June 27, 2005 at 15:56

How are you trying to communicate? Are you using the SPI or the UART peripheral? Which baud rate would you like to select?

yuanye-28
Associate II
Posted on August 10, 2005 at 06:07

The st7538's communication distance is 4-6km

Posted on August 29, 2005 at 08:12

are you sure?

How do you measure this?

reinhard_larch
Associate II
Posted on April 23, 2007 at 04:20

Hi,

I see a distance of a few hundred meters but with two entities only. As soon as there are more entities on the same network I only get 10-20m.

E.g. with 30 entities have a max distance of 15 meters. My system is based on 24VAC though, so maybe those values are different for 220VAC.

Regards

Reny

laurent239955_stm1
Associate II
Posted on April 23, 2007 at 09:19

Hi,

Thank you for using STMicroelectroinics products and website.

This forum is dedicated to ST7 microcontrollers.

You will get better support by contacting our technical support :

http://www.st.com/stonline/domains/support/contact_support.htm

Best regards

Laurent