cancel
Showing results for 
Search instead for 
Did you mean: 

SRAM memory

ezanen9
Associate II
Posted on October 04, 2005 at 13:26

SRAM memory

1 REPLY 1
ezanen9
Associate II
Posted on October 04, 2005 at 12:15

Hello, I am using an evaluation board with the STR710 microcontroller. For evaluation reasons I am running my programs from the SRAM memory which is 64kbyte. Till now no problem.

However I made a new program that is 95kbyte in size, I did not try it yet, but I think it is not possible to load into and run it from the SRAM now?

I can use the flash memory which is 256kbytes, but is it debuggable?

Jimmey