2005-09-06 06:12 AM
Some MB393 boards have USB defective!
2005-09-06 02:07 AM
I had a lot of problems with the USB on my MB393B v2.04! If you can't seem to make your USB work look at the D+ and D- signals (with a scope on resistors R13 and R14) and if they are both positive just replace the crap of circuit and put your own... it will work from first try.
2005-09-06 02:44 AM
Hi Tudor,
Yes , you are right it is possible to eliminate the USBUF01W6 IC which is only a USB filter IC , it was unfortunately uncorrectly mounted on the board. But we have done some tests, even mounted in the wrong way , the usb is still working fine. But as you mentionned , you could replace this chip by the pullup. Ciao Programmer2005-09-06 06:12 AM
On MB393-2.04 it looks to be mounted correctly, i've checked with it's datasheet. On my board it pulls up both D+ and D- so USB doesn't work fine anymore. What seems to me wrong is that the board was shipped to me not functioning... but anyway... it works now and I'm happy 😉
PS on another str710 board from hitex it's true that the links are done the other way round. Could that be the problem? There are just a couple of diodes in it... what could go so wrong with such a simple circuit?[ This message was edited by: tudor on 07-09-2005 10:27 ]