cancel
Showing results for 
Search instead for 
Did you mean: 

new member question

balaji_softproff
Associate II
Posted on September 16, 2005 at 05:53

new member question

1 REPLY 1
balaji_softproff
Associate II
Posted on September 16, 2005 at 05:53

hello everyone,

I got stpc atlas evaluvation kit. And i used primary loader and secondary loader downloaded from the stpc site.

my problem is, as per the document i should load my secondary loader at 80000h. when i did so it did not come. only my primary loader came up (this i saw thru the printouts from serial port).

After several test, this is my working condition,

My secondary loader is at c0000h.

I have to disable all cache and run it in the protected mode.

In 80000h when i enable cache(L1) the data at 80000h is wrong.

but when i disable the data is correct but not executing.

Can any one tell what is there between cache and 80000h location.

Wether my cache (l1) can be tested