cancel
Showing results for 
Search instead for 
Did you mean: 

OPTION byte AND TIMER SETTING

gianvin
Associate
Posted on October 14, 2005 at 08:59

OPTION byte AND TIMER SETTING

2 REPLIES 2
gianvin
Associate
Posted on October 04, 2005 at 17:42

Hello

if I program TIMER as OUTPUT MODE TOUT= 1

and DOUT =1 or DOUT = 0

should I program in the OPTION BYTE the TIM PULL bit as

0 (disabled)?

If I program as TIMER PULL UP =1 enabled what happen?

Destroy the device?

Increase the power consumption?

Thanks

Ghip

vikas2
Associate II
Posted on October 14, 2005 at 08:59

It will not cause any damage to the device but is not recommneded as pull up feature is for input mode(Tout = 0)

When Tout = 1 , the pull up is disabled even if the option is enabled.