cancel
Showing results for 
Search instead for 
Did you mean: 

STR710 with Greenhills Compiler

vaughan
Associate II
Posted on January 05, 2006 at 04:00

STR710 with Greenhills Compiler

2 REPLIES 2
vaughan
Associate II
Posted on January 03, 2006 at 19:37

Hi

I have been trying to get the ST lib's to work with the Greenhills compiler (Multi 2000 3.5). I have managed to get the example using interrupts to flash LEDs on the eval board working but can't get the UART interrupt example to work. It compiles ok but does nothing when it receives characters from the PC. I can see all the flags getting set correctly and the characters appearing in the buffer but nothing else happens. It works ok if I use the polling example.

What do I need to do to get the ST libs to work with Grrenhills?

Thanks

Vaughan

vaughan
Associate II
Posted on January 04, 2006 at 16:22

Hi

Thanks for that, worked great. What is special about this file and will it work for all the other interrupts?

Thanks

Vaughan