cancel
Showing results for 
Search instead for 
Did you mean: 

uPSD33xx VM reg

jim239955_stm1
Associate II
Posted on October 23, 2005 at 12:19

uPSD33xx VM reg

2 REPLIES 2
jim239955_stm1
Associate II
Posted on May 17, 2011 at 12:08

I had a rep tell me that the 3300 unit was easier to use for applications where you need to download new code to a unit in the field. He eluded to a change in the memory map logic that made this chip more flexable that the psd813F2 I was using.

Can anyone confirm this? I have looked in the manual but on a quick scan see no difference between the VM reg of a standard PSD part and the uPSD3354D series

jim239955_stm1
Associate II
Posted on May 17, 2011 at 12:08

So theres no truth to the claim that flash in program space can be programed? As in the original part, you must have the flash in data space to change it?