cancel
Showing results for 
Search instead for 
Did you mean: 

USB demo ported to FreeRTOS question

covertlife
Associate II
Posted on December 09, 2005 at 06:06

USB demo ported to FreeRTOS question

1 REPLY 1
covertlife
Associate II
Posted on December 09, 2005 at 06:06

im trying to port my current design to be used with the freeRtos (www.freertos.org/ ) Im using the example provided for the str7 Everything is working expcept the usb. So far i have the irq handlers for the uarts. is there any other irq handling that im missing for the usb? i noticed the USBLP_Addr intterupt doesn't occur during a pc/usb negotiation, so there must be something else.

ive attached the freertos and the usb demo version of the vect.s79 files, is there a simple way anyone knows to convert the usb demo vector file to be used in the freertos version vector file. also anyone have any suggestions on other free rtos' to use.

thanks for any help.

________________

Attachments :

vect1.s79 : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtSp&d=%2Fa%2F0X0000000aQK%2FKPqy8w15DAoanX59sq7L8O318fHe6oJJUTDI1DcrO34&asPdf=false

vect2.s79 : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtSu&d=%2Fa%2F0X0000000aQL%2F9dkQDnDup64dm68vjFW5TAie4ny2JZEhZVqzzjIv_pc&asPdf=false