cancel
Showing results for 
Search instead for 
Did you mean: 

MMC or SD card in SPI mode with STR710

julienduay
Associate II
Posted on February 16, 2006 at 07:12

MMC or SD card in SPI mode with STR710

4 REPLIES 4
julienduay
Associate II
Posted on February 15, 2006 at 05:29

Hello everybody.

Can I transfer data on a MMC or SD memory card (in SPI mode) with the BSPI interface of STR710 micro-controller?

Thank you

fa
Associate II
Posted on February 15, 2006 at 06:29

Yes, it is possible.

julienduay
Associate II
Posted on February 15, 2006 at 10:15

Thank you for your answer.

Did you already use SPI signals for reading and writing on a SD card?

Is there a free example on the Web for the memory card driver?

fa
Associate II
Posted on February 16, 2006 at 07:12

Look at

http://www.ulrichradig.de/

best regards, Frank Andersen