cancel
Showing results for 
Search instead for 
Did you mean: 

STR7-EVAL Programming & Debugging

gwilson
Associate II
Posted on May 05, 2006 at 13:57

STR7-EVAL Programming & Debugging

6 REPLIES 6
gwilson
Associate II
Posted on March 16, 2006 at 12:11

I currently have a STR7-EVAL board and Microcross GNU X-tools and Nohau EMUL-ARM development tools. I am new to the ARM development environment and was wondering what other tools are needed to utilize this development board.

Appears I might need to purchase the rlink for programming.

sam5
Associate II
Posted on March 23, 2006 at 14:31

Folks,

I am in the same boat. I have STR710 EVAL board with no

documenation and seems like no firmware loaded in it?

Also I have RLink JTAG dongle and RFLasher tool.

I want to use GNU tools and working on uclinux / eCOS related

things.

Now I want to know if using Rlink I can program?

1. Internal flash on STR710.

2. External Flash on STR710 board.

3. External SRAM on STR710 board.

Thanks

sam

gwilson
Associate II
Posted on March 27, 2006 at 13:02

I have a manual for the STR710-EVAL and there is demostration software on the board. It appears the demo software is being run from internal flash is this correct and is there source code for the demostration software available?

gwilson
Associate II
Posted on March 27, 2006 at 14:14

So if I would program the internal flash for my application there would be no way to reload the demostration program.

gwilson
Associate II
Posted on May 05, 2006 at 11:23

Is it possible to get STR710-EVAL board's demo software in elf format? Instead of axf.

gwilson
Associate II
Posted on May 05, 2006 at 12:14

I am currently using seehau EMUL-ARM with the EMUL-PC/USB-JTAG interface to download to the MB393B board. Apparently, the axf format is not supported by seehau.

I really don't want to buy another development system at $2000 a pop to work with STMicroelectronics MB393B board.