cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 Visual Develop and Vista

dpeter
Associate II
Posted on November 06, 2007 at 09:27

ST7 Visual Develop and Vista

2 REPLIES 2
dpeter
Associate II
Posted on October 06, 2007 at 01:50

When I try to compile with ST7 VD (Cosmic Compiler) with Vista, I get the following errors.

access to default.wed is denied

can't create *.cx1

Any ideas??

Thanks

Dave P

sg2
Associate
Posted on November 06, 2007 at 09:27

Quote:

can't create *.cx1

that is a problem by having no write accress to the temporary used directory - normaly the compiler use the %windows%\temp folder

(older compiler versions use root)

alternative you can set that - using option cxst7.exe -t

make sure you have write access to the path