cancel
Showing results for 
Search instead for 
Did you mean: 

problem with worskspace ST7FLITE20

qcalv
Associate
Posted on May 04, 2006 at 15:14

problem with worskspace ST7FLITE20

2 REPLIES 2
qcalv
Associate
Posted on April 28, 2006 at 09:06

Hi,

I have a problem with ST7DV and i didn't find how to solve it. I tried almost everything. When i create a workspace i have no problem, then when i want to debug my asm i press start debugging and then i select which window i want to see ( like ST7 register) but then when i press stop debugging i have an error message saying ''Unable to save workspace.'' with a red cross, and of course when i press one more time debug, i lost all my window positions. i tried to reinstall the program, to see if the read/write protection from windows was activated, and i tried to boot my computer with windows and only what i needed, but sadly always this message ?

Anyone has any idea ? :o

Thank you.

alain2399
Associate II
Posted on May 04, 2006 at 15:14

Very strange behavior.

Can you reproduce it with the ADC example provided with STVD7 using the assembler project inside this ADC workspace ?