2007-12-19 05:20 PM
2006-05-05 10:25 AM
Hi guys! I'm trying to write and after read some data from Serial Flash memory. I use STR710FZ2T6.
My problem is: I can't neither read nor write data in flash. Well, I will post my source. I'll appreciate any answer or advices. Sorry for my bad english! // Stop flash for configuration // Everytime you wanna to send a command to flash you must call the Spi_Flash_SSN_Low() Spi_Flash_SSN_High (); // Initialize Spi-Flash (configure pin and set BSPI1 as master) Spi_Flash_Init(); // Init and configure BSPI1 Bspi_Disable ( BSPI1 ); BSPI1->CSR1 = ( BSPI_MASTER_SELECT | BSPI_8_BIT_WORD_LENGTH ); BSPI1->CSR2 = BSPI_RESET_FIFO; Bspi_Clockivider (BSPI1, 8); //BSPI1->CSR1 |= BSPI_10_WORD_Rx_FIFO_ENABLE; //BSPI1->CSR2 |= BSPI_10_WORD_Tx_FIFO_ENABLE; Bspi_Enable ( BSPI1 ); /*****************************************************************************/ // Start communication // Write enable instruction Spi_Flash_SSN_Low (); Spi_Flash_SendInstruction ( M25_WREN ); Spi_Flash_SSN_High (); // Erase sector before record data in memory Spi_Flash_SectorErase ( M25_Sector3 ); // Send a Read Status register instruction in order to see if the erase already was done Spi_Flash_WaitBusy (); // Write enable instruction Spi_Flash_SSN_Low (); Spi_Flash_SendInstruction ( M25_WREN ); Spi_Flash_SSN_High (); // Start writing Spi_Flash_SSN_Low (); Spi_Flash_SendInstruction ( M25_PP ); Spi_Flash_SendAddress ( 0x00000 ); for (int i=0; i Spi_Flash_SendData(0xAA); Spi_Flash_SSN_High (); // Wait instruction to be completed Spi_Flash_WaitBusy (); // Write Enable Spi_Flash_SSN_Low (); Spi_Flash_SendInstruction ( M25_WREN ); Spi_Flash_SSN_High (); //Spi_Flash_WriteStatusRegister ( 0x0C ); //Spi_Flash_WaitBusy (); //bb = Spi_Flash_ReadStatusRegister(); // Read data to see if it was correctly recorded into spi-flash memory Spi_Flash_SSN_Low (); Spi_Flash_SendInstruction ( M25_READ ); Spi_Flash_SendAddress ( 0x00030 ); // Receive all the data sent in reverse order for (int i=9; i>=0; i++) Buffer[i] = Spi_Flash_ReceiveData(); Spi_Flash_SSN_High (); while(1); // infinite loop inline void Spi_Flash_Init () { // Configure GPI00 on mode Alternate function Push Pull GPIO_Config ( GPIO0, BSPI1_MISO | BSPI1_MOSI | BSPI1_SCLK, GPIO_AF_PP ); // Configure SCLK & SSN clock and data lines control GPIO_Config ( GPIO0, M25_SSN | BSPI1_MC | BSPI1_SSN, GPIO_OUT_PP ); // Set the BSPI1_MC pin to high level to configure the BSPI1 as master in the STR710 eval board GPIO0->PD |= 0x0002; } // Everytime you wanna to send a command to flash you must call the Spi_Flash_Enable() // that keep the !SSN M2510 pin low inline void Spi_Flash_SSN_Low () { GPIO0->PD &= ~0x0008; } // And after any access you gotta set high !SSN pin calling Spi_Flash_Disable inline void Spi_Flash_SSN_High () { GPIO0->PD |= 0x0008; } u8 BPSI_DataSendReceive ( u8 data ) { u8 ret_value; while( BSPI1->CSR2 & BSPI_Rx_FIFO_NOT_EMPTY ) ret_value = BSPI1->RXR; // Clear Rx FIFO // Wait until the Transmit FIFO is empty while( !( BSPI1->CSR2 & BSPI_Tx_FIFO_EMPTY ) ); // Send data to Transmit buffer BSPI1->TXR = (data< // Wait until the Transmit FIFO is empty while( !( BSPI1->CSR2 & BSPI_Tx_FIFO_EMPTY ) ); // Wait until the end of transmission while( BSPI1->CSR2 & BSPI_Rx_FIFO_NOT_EMPTY ) ret_value = BSPI1->RXR; // Clear Rx ret_value = (BSPI1->RXR)>>8; // Read the received data return ret_value; } inline void Spi_Flash_SendAddress ( u32 data ) { Spi_Flash_SendData ( (data & 0x00FF0000)>>16 ); Spi_Flash_SendData ( (data & 0x0000FF00)>>8 ); Spi_Flash_SendData ( (data & 0x000000FF) ); } inline u8 Spi_Flash_ReadStatusRegister() { u8 ret_value; // Select device Spi_Flash_SSN_Low(); // Send instruction to Transmit buffer ret_value = BPSI_DataSendReceive ( M25_RDSR ); // Deselect device Spi_Flash_SSN_High (); return ret_value; } inline void Spi_Flash_WriteStatusRegister ( u8 value ) { // Select device Spi_Flash_SSN_Low(); // Send instruction to Transmit buffer BPSI_DataSendReceive ( M25_WRSR ); BPSI_DataSendReceive ( value ); // Deselect device Spi_Flash_SSN_High (); } inline void Spi_Flash_SectorErase ( Spi_Flash_Sector_TypeDef Sector ) { // Select device Spi_Flash_SSN_Low(); // Send Sector Erase Instruction BPSI_DataSendReceive ( M25_SE ); // Send sector address Spi_Flash_SendAddress ( Sector ); // Deselect device Spi_Flash_SSN_High (); } inline void Spi_Flash_WaitBusy() { while ( ( Spi_Flash_ReadStatusRegister() & M25_WIP ) ); } Thanks!! 😉2006-05-08 07:41 AM
Hi!
I can read any memory position, including the Eletronic Signature through an instruction. But my writes appear don't have effect. I also erased all memory using Erase Bulk. So, I just can read 0xFF. I use the same routine for read and write: u8 BPSI_DataSendReceive ( u8 data ) { u8 ret_value; while( BSPI1->CSR2 & BSPI_Rx_FIFO_NOT_EMPTY ) ret_value = BSPI1->RXR; // Clear Rx FIFO // Wait until the Transmit FIFO is empty while( !( BSPI1->CSR2 & BSPI_Tx_FIFO_EMPTY ) ); // Send data to Transmit buffer BSPI1->TXR = (data< // Wait until the Transmit FIFO is empty while( !( BSPI1->CSR2 & BSPI_Tx_FIFO_EMPTY ) ); // Wait until the end of transmission while( !(BSPI1->CSR2 & BSPI_Rx_FIFO_FULL) ); ret_value = (BSPI1->RXR)>>8; // Read the received data return ret_value; } And SW7 and SW8 are OK! Memory is not hold neither hardware protected against write. That's it! Tks!2006-05-08 09:33 AM
I solved the problem! Tks! 😉
2006-05-09 12:58 AM
Sure! Actually my source is a little different now! But the main reason is that I was verifying the WIP (Write in progress) bit of serial flash in a wrong way. Because I forgot to discard some dummy byte after the Read Status register command. The correct way to verify is:
void Spi_Flash_WaitBusy() { u8 status = (Spi_Flash_ReadStatusRegister() | M25_WIP); while ( (status & M25_WIP) ) status = Spi_Flash_ReadStatusRegister(); } u8 Spi_Flash_ReadStatusRegister() { u8 ret_value; // Select device Spi_Flash_SSN_Low(); // Send instruction to Transmit buffer and receive Status Register Spi_Flash_SendInstruction ( M25_RDSR ); ret_value = Spi_Flash_ReceiveData(); // Deselect device Spi_Flash_SSN_High (); return ret_value; } That's it RISC! Tks!2006-10-04 08:58 PM
Hello Rickyson!!!
Can you please give me your source code for using the spi flash...I also am using the spi flash M25P32.Is there any difference??? I would be thankfull to you. Thanks in advance. Sany2007-12-19 05:20 PM
Hello,
I am also struggling to read and write into M25P64 flash through SPI0. Please send me sample source code if you have,,,, rajendrask@hcl.in