cancel
Showing results for 
Search instead for 
Did you mean: 

the interrupt of 3434

xmwang
Associate
Posted on July 03, 2006 at 00:06

the interrupt of 3434

1 REPLY 1
xmwang
Associate
Posted on May 17, 2011 at 11:50

I used the 24MHz crystal for system and the work is ok.

when I want to change the 24MHz to 3.6864MHz, the interrupt of EXTINT0 will not respond correctly,it seems that some interrupt is not be responded.For the EXTINT0 is set to edge and the external interrupt will keep 1us low level, Is there some problems?