cancel
Showing results for 
Search instead for 
Did you mean: 

What is the purpose of SRAM_SIZE option in STR91 series

nanuradha
Associate II
Posted on September 12, 2006 at 06:01

What is the purpose of SRAM_SIZE option in STR91 series

2 REPLIES 2
nanuradha
Associate II
Posted on May 17, 2011 at 09:32

In the reference manual SRAM_SIZE option is there.In what application is that useful.Is there any restriction depending on SRAM size on other features.

Regards

Anuradha.

kais
Associate II
Posted on May 17, 2011 at 09:32

Hi anuradha,

After reset the size of the on-chip SRAM is limited to 32K .among STR9 features :the configurable size of its SRAM (32K, 64K,96K).So it depends on the complexity of your application to select a large size : Application including RTOS, TCP/IP stack…

Regards

Eris.