cancel
Showing results for 
Search instead for 
Did you mean: 

STR9 with Keil-Kit problem

dmaiocchi9
Associate II
Posted on October 09, 2007 at 16:37

STR9 with Keil-Kit problem

2 REPLIES 2
dmaiocchi9
Associate II
Posted on May 17, 2011 at 09:47

Hi,

i'm a new to use STR9- ARM with KEIL kit: STR91X-SK/KEI/A.

When i startup the µVISION3 it stop loading with this error :''Eccezione WIn32 in armcc.exe''

I have ''Microsoft Windows XP Professional 2002 Service Pack 2'' original. Intel Pentium 4 CPU 2.53GHz

Can you help me.....

sarao
Associate II
Posted on May 17, 2011 at 09:47

I was recently getting this problem. Here are the steps I used to ''fix'' the problem:

1. I deleted all the .dep and .Bak files from the directory that my .Uv2 project file was in.

2. I also deleted all the listing files and output files (there was no need for me to keep them around anyway)

3. I then rebooted.

4. Opened up my .Uv2 file and was able to compile without problem.