cancel
Showing results for 
Search instead for 
Did you mean: 

RLink and Ignore Options Bytes

peterwrigley9
Associate II
Posted on December 07, 2006 at 14:11

RLink and Ignore Options Bytes

2 REPLIES 2
peterwrigley9
Associate II
Posted on December 07, 2006 at 11:23

Hi all,

I am using an ST7FLITES5Y0 with STVD7 3.3.3. I have programmed the hardware watchdog option, and despite setting the IDE to ignore option bytes the device will not program. When I tell the IDE to use the option bytes I get the known warning about the hardware watchdog. When I tell it to ignore the bytes it ''fails to download monitor''. Both problems only manifested after setting the hardware watchdog. I am using one of the 'new' RLinks.

I can't work out where the problem is!

peterwrigley9
Associate II
Posted on December 07, 2006 at 14:11

Sorry boys

I've got a confobulator board with the target board and I think the pinout may be incorrect.