2008-06-05 02:45 AM
Program stuck when exiting from stop mode
2008-05-26 10:29 PM
I worked with STR751, IAR compiler and have problem with some device to exit from stop mode (LP_PARAM15) .
I found that the device wake up from interrupt (EXTIT_ITLine15 (wake up) or EXTIT_ITLine4 (external interrupt line 4)), But it didn’t return to the program from the interrupt and it go to PrefetchAbortHandler in some devices or to SWIHandler in others. It seems like the lr or the pc registers are damaged. Do you have any suggestion what wrong? How I handle with Prefetch Abort, SWI Interrupt, (is there an example). Thanks in advance.2008-06-05 02:45 AM
you can add a code in the PrefetchAbort handler to recover as generate a system reset or other code for debugging. You can refer to STR75x Low Power Application note
http://www.st.com/mcu/familiesdocs-86.html
which provides example of Stop mode configuration in case of miss configuration 😉