cancel
Showing results for 
Search instead for 
Did you mean: 

GPIOINx in CAPS?

ken
Associate II
Posted on December 07, 2006 at 14:24

GPIOINx in CAPS?

1 REPLY 1
ken
Associate II
Posted on May 17, 2011 at 09:34

Yesterday I started using the CAPS tool (ver 2.30) for an STR911FM44 with the stdlib code. I have the include files and paths all set up correctly. However, I get about 20 unresolved variable errors when I compile 91x_conf.c. The errors have to do with pins which are not found on the 80 pin package (ports 0, 1, 7, 8, 9, etc.).

Is there a version of 91x_conf.c for the 80 pin package or do I need to manually edit the one I downloaded?

Thanks for any help which you may be able to provide.