cancel
Showing results for 
Search instead for 
Did you mean: 

MircorFramwork

kjepsen9
Associate II
Posted on July 27, 2009 at 19:08

MircorFramwork

6 REPLIES 6
kjepsen9
Associate II
Posted on May 17, 2011 at 13:18

Hello,

Just now we are talking about uC linix...

Has anyone thought about port the MS Microframework?

I defently think it is possibly to run on the 3210E Eval board.

Howcome all the external RAM/Flash is taken of the new Eval board for connectivity line?

Kasper

st3
Associate II
Posted on May 17, 2011 at 13:18

Quote:

I defently think it is possibly to run on the 3210E Eval board.

On what basis do you think that?

kjepsen9
Associate II
Posted on May 17, 2011 at 13:18

These ppl can do it:

http://www.ghielectronics.com/product/113

Kasper

st3
Associate II
Posted on May 17, 2011 at 13:18

Quote:

These ppl can do it:

http://www.ghielectronics.com/product/113

Yes - but on different hardware.

Have you specifically verified that the 3210E Eval board has the necessary resources to support the micro framework?

In fact, what are the minimum resources necessary to support the micro framework?

[ This message was edited by: st7 on 24-07-2009 18:37 ]

16-32micros
Associate III
Posted on May 17, 2011 at 13:18

Hi,

You can visit

http://www.microsoft.com/netmf/hardware/default.mspx

http://www.microsoft.com/downloads/details.aspx?displaylang=en&FamilyID=42ce8508-ff00-4ab8-8495-df587d77a8f2

The Micro Framework Porting Kit supports the adaptation of the platform to specific hardware for processors using the RealView, Keil and GCC toolchains for the ARM processors (including Cortex)...

Cheers,

STOne-32.

kjepsen9
Associate II
Posted on May 17, 2011 at 13:18

Hello,

No, but compared to the specs in the link i gave the 3210E eval board has many more features + RAM/ROM...

And the other i believe is the ARM7TDMI..

Kasper