cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with C Code Generation in PSDsoft Express

diego239955
Associate II
Posted on March 23, 2007 at 08:07

Problems with C Code Generation in PSDsoft Express

1 REPLY 1
diego239955
Associate II
Posted on May 17, 2011 at 11:51

I have started to work with PSDsoft Express, and i 'm doing the example in the AN 1560. All is right, but in the moment when i must do the C Code, i have problems, when I push the bottom ''Generate C code, Specific to PSD''. It appears to me a pop up with this message ''Please check the website listed below for the latest firmware updates:'' and two links. These links are:

http://mcu.st.com/mcu/modules.php?name=Content&pa=showpage&pid=55

http://mcu.st.com/mcu/modules.php?name=Content&pa=showpage&pid=56

What is the problem, and what is the solution?

I wish create a C code, but i don't understand if I must make the code with this option, or with Keil.

Thanks very much.