cancel
Showing results for 
Search instead for 
Did you mean: 

STR750 : TIM PWM input capture (with PWM signals < 2kHz)

xaviooo
Associate II
Posted on June 14, 2007 at 08:40

STR750 : TIM PWM input capture (with PWM signals < 2kHz)

2 REPLIES 2
xaviooo
Associate II
Posted on June 12, 2007 at 14:24

Hello everybody,

Using the Timer PWM input capture example, i'm trying to get the duty cycle of a PWM signal whose frequency is below 2kHz with CK_TIM = 60 MHz.

It works when f > 2kHz, but not with a 1800 Hz signal.

Thank you for your help.

-Xavier

kaouther
Associate II
Posted on June 14, 2007 at 08:40

Hello,

- using CK_TIM = 60 MHz, it is possible to measure the frequency and

duty cycle of a PWM signal frequency of 915Hz.

what is the prescaler value set when measuring the 1800Hz signal?