cancel
Showing results for 
Search instead for 
Did you mean: 

Error in programming str711x with jtag

quentin239955
Associate II
Posted on November 26, 2007 at 14:14

Error in programming str711x with jtag

1 REPLY 1
quentin239955
Associate II
Posted on November 26, 2007 at 14:14

Hi !

I have problem in programming my project hardware (based on str711x) with JTAG (realviem ICE) from Realviem.

When I want to program (after choosing my .axf file and pressing write) I get this message :

''Failed writing to Flash block 0, offset=0 - flash returned 01''

and then this one :

''Error V003D (Vehicle): Failed writing cache to Flash''

This worked fine before, and I don't think that the flash reached his max cycles limit.

Is anyone more familliar than me with this environnement and hopefully this error message ?

And I also wanted to know about the connection properties : Is-it usefull to create a specific one for each project ? I allways used ARM-ARM-USB->ST-STR710FZ2->ARM7TDMI0 and it worked fine, but with my actual problem, I suspect this...

Thanks in advance !