cancel
Showing results for 
Search instead for 
Did you mean: 

Program ST10R167

fabien2
Associate II
Posted on May 30, 2007 at 07:38

Program ST10R167

3 REPLIES 3
fabien2
Associate II
Posted on May 29, 2007 at 12:27

Hello,

I'm new and I have a question of beginner.

So I have a ST10R167 and I wish to program it. If I have understood, this ic have an internal rom and I have already an ic programmed.

Can I recover his program to send it in another empty ic ?

If yes, which software could I use to ?

Can I use the software st10flasher 2.4 ?

Can I use a converter base DIL48/PQFP144 to program it (because I have

a device programmer DIL48)?

Is it possible that I cannot read the program (program locked in reading) ?

In fact, I just want to copy/stick the program.

Thank you for your answer.

fabien2
Associate II
Posted on May 30, 2007 at 05:29

Hello Neila,

Thanks for your quick answer but I don't understand !

Here it is the block diagram, and you can see just like me an internal rom

takes part in the functional mode of the ST10R167-Q3.

ST10R167 > R for ROM

ST10F... > F for FLASH

Could you explain to me ?

Thanks.

________________

Attachments :

SurveyReport_1_.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0NN&d=%2Fa%2F0X0000000bYB%2FtvrzSGr90DQVqPhQkGMGrsZvO6yOLLIcfMH6M0XAeCg&asPdf=false
fabien2
Associate II
Posted on May 30, 2007 at 07:38

If I do understand this time the references has changed

In the past the ST 10 R 167 was different

because the block diagram I possess puts to light an internal rom

and it's not the case any more. So the generic family ST 10 X makes now a difference with the last generation of chips.

Is it all right if I replace now an OLD ST10R167 by a NEW ST10C167 ?

And what would be the software to be used for programming it ?

Thank you for your answer