cancel
Showing results for 
Search instead for 
Did you mean: 

Math Co Processor for STR7

hugo123
Associate
Posted on June 13, 2007 at 14:22

Math Co Processor for STR7

2 REPLIES 2
hugo123
Associate
Posted on June 13, 2007 at 11:50

Hello, on the homepage of ARM stands that the ARM7TDMI has an interface for a COprocessor. Is it possible to attach to the STR7 mathematical CO a processor?

Are there are any restrictions, which coprocessor I can use. And wheredo i get such Co-Processors?

[ This message was edited by: hugo123 on 13-06-2007 15:34 ]

sofiene
Associate III
Posted on June 13, 2007 at 14:22

Hi hugo123,

I think that ARM7TDMI core built in STR7 is isolated from the extern environnement (the microcontroller package), so I think that there are no external interface to a specific co-processor. However, if there are any co-processor which able to communicate with EMI (External Memory Interface), I think it is possible in this case to interface it with STR710 EMI interface.