cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with st10f269

wizard1
Associate
Posted on June 14, 2007 at 13:01

Problem with st10f269

1 REPLY 1
wizard1
Associate
Posted on June 14, 2007 at 13:01

I am planning to use the HOLD/HLDA bus sharing mode on the ST10F269 so that another CPU can write into XRAM on the ST10's bus.

I use ST10F269 Microcontroller Slave mode

The ST10F269 works with the program in the inside flash

Signals pins:

ST10F269(EA=1)

ST10F269(HLDA=1)

CPUmaster(CS) >>> ST10F269(Hold)

CPUmaster(RD) >>> ST10F269(RD)

CPUmaster(WR) >>> ST10F269(WR)

CPUmaster(16bit data) >>> ST10F269(16bit data)

CPUmaster(address) >>> ST10F269(address)

Problem:

if the slave(ST10F269) read xram when it enters hold mode and the master write in the xram, the data they are introduced an one wrong address