cancel
Showing results for 
Search instead for 
Did you mean: 

ERASE FLASH

newsamo
Associate II
Posted on September 18, 2008 at 02:24

ERASE FLASH

3 REPLIES 3
newsamo
Associate II
Posted on May 29, 2008 at 10:28

I'm working on st10f168 with st10flasher, now, load monitor is ok, dump is ok, but i'm not able to program flash because appears error messagea boute flash erase: EraseFlash failed.flash

How can i erase ?

najoua
Associate II
Posted on June 02, 2008 at 07:05

Hello Newsamo,

Programming voltage (12V) of the on-chip Flash memory must be supplied to pin VPP(pin 84).

Is the 12V ensured in this pin during programming/erasing operation?

Best regards,

Najoua.

joluci
Associate
Posted on September 18, 2008 at 02:24

Hello Najoua,

in which others microcontrollers of st10fxxx family I need to apply the voltage programming to erase and program?

Thank you !!!