cancel
Showing results for 
Search instead for 
Did you mean: 

Core does'nt wake up

netz
Associate II
Posted on August 14, 2008 at 05:49

Core does'nt wake up

1 REPLY 1
netz
Associate II
Posted on August 14, 2008 at 05:49

Hello,

I'm searching for a advice for debugging.

In a application, I receive via UART1 characters

in the FIFO through UART_RxHalfFull.

It set a Message to a Task to calculate the chars.

At the end of the Task, the Interrupt UART_RxHalfFull

will be set again.

Code:

ISR:

{

UART_ItConfig(UART1,UART_RxHalfFull|UART_TimeOutNotEmpty, DISABLE);

SetMessage(ProcessChars);

}

Task:

if ( ProcessChars)

{

while (UART1->SR & UART_RxBufNotEmpty ) {

ProcessChars;

}

UART_ItConfig(UART1,UART_RxHalfFull|UART_TimeOutNotEmpty, ENABLE);

/* Reset bit WFI in the RCCU_SMR register */

RCCU->SMR &= 0xFE ;

}

[/CODE]

It runs, as expected. But after a random count,

the core does'nt wake up, and I get the UART_OverrunError.

How can I debug, the wakeup of the core?

I can see the timing per IO-Ports on the Oszi.

But why does'nt wake up the core sometimes.

Any idea?

Thanks,

Steffen