2008-01-20 06:44 PM
2008-01-06 11:14 PM
We purchased an STR710-EVAL board and loaded into it the uCLinux, downloadable from the ST page.
As the linux boots, the ports 2.12, 2.13 and 2.14 begin to act as a counter and are counting from 0 to 7. These ports are associated to 3 leds, so I see the 3 leds blinking and counting. We will build our own board with an STR710 core and uCLinux and we do need these ports. Is there any way to disable this counting?2008-01-15 05:37 AM
Dear avelez,
You may change the led blinking example by modifying the arch.c file under ''linux-2.4.x/arch/armnommu/mach-STR710/arch.c '' directory. 😉2008-01-15 07:49 PM
Hi coucou,
Thanks for your reply. However, in that file only that content is shown: -------- #include linux/tty.h #include linux/delay.h #include linux/pm.h #include linux/init.h #include asm/elf.h #include asm/setup.h #include asm/mach-types.h #include asm/mach/arch extern void genarch_init_irq(void); MACHINE_START(STR710, ''STR710'') MANTAINER(''ST MMCC'') BOOT_PARAMS(0x00000100) INITIRQ(genarch_init_irq) MACHINE_END ---- I cannot see where should I modify the file :( [ This message was edited by: avelez on 16-01-2008 09:19 ] [ This message was edited by: avelez on 16-01-2008 09:20 ] [ This message was edited by: avelez on 16-01-2008 09:21 ]2008-01-16 02:54 AM
Yes, not the arch.c but the time.c and time.h instead. Hope it helps;
linux-2.4.x/arch/armnommu/mach-STR710/time.c linux-2.4.x/include/asm-armnommu/arch-STR710/time.h2008-01-20 06:44 PM
Yes!! It definetely works!! Thanks a lot for the info 😉