cancel
Showing results for 
Search instead for 
Did you mean: 

Can't uncompress ucLinux Kernel

henzaimz1
Associate II
Posted on September 21, 2007 at 04:22

Can't uncompress ucLinux Kernel

3 REPLIES 3
henzaimz1
Associate II
Posted on September 19, 2007 at 10:27

I'm deverloping a STR710 kit base on STR710-Eval but with

zimage.bin downloaded from ST, i can't uncompress ucLinux Kernel :(

All file have loaded successful, but the line: ''Uncompressing Linux ...... done'' didn't apprear.

My system EMI consist of:

1Mx16 External SRAM

2Mx16 External FLash

With that configuration, must i change source code in STR710-Eval Bootloader?

[ This message was edited by: henzaimz on 19-09-2007 14:00 ]

henzaimz1
Associate II
Posted on September 20, 2007 at 03:09

I loaded STR710-Eval bootloader into Internal flash and then used it to load itself( bin image file ) into 0x60000000 of EMI(begin of External Flash). Then i set to boot system from EMI and couldn't uncompress ucLinux :(

Help me!!!

henzaimz1
Associate II
Posted on September 21, 2007 at 04:22

Hi all :D

My problem is the Bootloader and ucLinux original images(downloaded from ST website) are configed to run with STR710-Eval, I added one 1Mx16 SRAM and it worked well :D