cancel
Showing results for 
Search instead for 
Did you mean: 

STR750MCKIT

kstin
Associate
Posted on December 06, 2007 at 05:49

STR750MCKIT

2 REPLIES 2
kstin
Associate
Posted on December 05, 2007 at 10:58

Hallo,

I want to debug the provided software for PMSM motors. If I tried to execute ''rebuild all'' in IAR Embedded Worckbench it shows me some errors:

Error[109]: Expression is too complex K:\projekt\STR750_servo\IAR_infos\foc_pmsm\FOC_PMSM_SR_v1.1\IAR\config\75x_init.s 250

Error while running Assembler

75x_it.c

75x_pwm.c

75x_tb.c

75x_vect.s

Error[40]: Bad instruction K:\projekt\STR750_servo\IAR_infos\foc_pmsm\FOC_PMSM_SR_v1.1\IAR\config\75x_vect.s 21

Error while running Assembler

MC_Display.c

after i tried to debug software, the demo software on the eval.board dosn't work anymore. and I cold not to reprogram this. It shows me: Bad JTAG communication: Write to IR: Expected 0x1, got 0x7(TAP Command:2)@ Off 0x5.

How can i solve this problem?

zouhair
Associate II
Posted on December 06, 2007 at 05:49

Hi,

It seems that you are using the new version of EWARM 5.10A. And in this case you need to update the assembler files and use the new linker file(*.icf).

Those files are available under:

''C:\Program Files\IAR Systems\Embedded Workbench 5.0 \ARM\examples\ST\STR75x\STR75xLibrary''

Rgds,

Zouhair