cancel
Showing results for 
Search instead for 
Did you mean: 

STR712FR2: problems with interrupts while running from RAM...

pshtaferun
Associate
Posted on December 07, 2007 at 10:11

STR712FR2: problems with interrupts while running from RAM...

2 REPLIES 2
pshtaferun
Associate
Posted on December 04, 2007 at 07:41

Dear All,

I have encounered a problems with interrupts while running code from RAM...

Environment:

Keil uVision 3.55a and MDK 3.15b

I took an example from Examples\ST\STR71xLib\Tim\OCMP and changed it in the way to work in RAM.

What i see is that Timer 3 output compare function pin triggers but interrupt routine doesn't work (there are no port pins toggling)...

When i run it in debug mode (using the internal uVision debugger) all seems to be working...

Does anybody encounter with such problems before?

I would be very appreciated for your help.

P.S.Source code i'm experimenting with is attached for your consideration...

Thank you.

________________

Attachments :

OCMP.ZIP : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1NS&d=%2Fa%2F0X0000000bmC%2FqFJqRlnvhC9zyQOZAYNG8KIfJK7mU4OgE2s.E_r4d7Q&asPdf=false
christophe239955_st
Associate II
Posted on December 07, 2007 at 10:11

I have an STR710 interrupt example running from RAM and the porject setting is different than yours. you can check also the boot pin on your board. I attached my setting. Hope this helps you,

Cheers,

Chris.

[ This message was edited by: christophe.beyen on 07-12-2007 14:43 ]

________________

Attachments :

project-setting.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtQZ&d=%2Fa%2F0X0000000aPs%2Fmnzo5O4R9sLjnD3M8kBe.y98FobZG6VD6elw6H1kIUQ&asPdf=false