cancel
Showing results for 
Search instead for 
Did you mean: 

PSRAM with burst mode vs. fast SRAM

alexanderpapsdorf9
Associate II
Posted on February 05, 2009 at 06:35

PSRAM with burst mode vs. fast SRAM

1 REPLY 1
alexanderpapsdorf9
Associate II
Posted on May 17, 2011 at 09:57

Hello,

For an application with STR9 we have to design a board with external RAM. We are not sure, if we should use PSRAM instead of SRAM. The price for the external memory is secondary. For our application, speed is more important. We would like to access the external memory in 16 bit muxed mode. The question is, which memory gives us in average a better performance, a SRAM with an access time of 12ns or a PSRAM with 70 ns access time and burst mode feature?

Thanks

Alex