cancel
Showing results for 
Search instead for 
Did you mean: 

TFT LCD interfacing with the high-density STM32F10xxx FSMC

clara
Associate II
Posted on April 21, 2009 at 08:06

TFT LCD interfacing with the high-density STM32F10xxx FSMC

2 REPLIES 2
clara
Associate II
Posted on May 17, 2011 at 13:09

Hi,

I'm working with the STM3210E-EVAL board and RIDE7 with Rlink-PRO from RAISONANCE. I've downloaded the firmware of the ''AN2790: TFT LCD interfacing with the high-density STM32F10xxx FSMC'' and when I try to run the application it doesn't work. When the program is configuring the GPIOs, a ''HardFaultException'' appears and the program starts an infinite loop. I've just followed the written instructions in the readme.txt without any change :o

Just in case, I have to say that I can run the examples of the FW library.

Thanks.

clara
Associate II
Posted on May 17, 2011 at 13:09

Hi,

The problem is solved. I've updated the RIDE7 and RKit-ARM to the last versions and the demo works without problems :-]

Bye.