cancel
Showing results for 
Search instead for 
Did you mean: 

Library USART upsd3434EV

marcotorelli81
Associate II
Posted on May 13, 2009 at 07:18

Library USART upsd3434EV

1 REPLY 1
marcotorelli81
Associate II
Posted on May 17, 2011 at 11:52

Good morning,

I am using the upsd3434EV with the crystal of 40MHz, I am using the library USART to communicate with a PC through COM, I want to use a BaudRate of 115200. Using the library for the UART taken from the site at the BaudRate of 19200 works without problem, when increase the BaudRate ones beyond 19200 in order to go up does not work more the USART. I am using the code written from Mark To. Odell, I use the compiler RIDE last version with RLINK. Any solution?

Thanks to all in advance for l' aid.

Marco

[ This message was edited by: marcotorelli81 on 13-05-2009 10:49 ]