cancel
Showing results for 
Search instead for 
Did you mean: 

Are there any difference between SPI0 and SPI1???

oe
Associate II
Posted on May 25, 2009 at 07:59

Are there any difference between SPI0 and SPI1???

1 REPLY 1
oe
Associate II
Posted on May 17, 2011 at 09:58

I need to use SPI1 an a motorola style master, but I can't recive. If I use the same code on SPI0 it works fine.

I can set SPI1 in loopback mode.

I have verifeid the electrical stuff.

I use P3.6 and P3.7.

Is there anyone that have experience of SPI1 at P3??

Regards

Ola