cancel
Showing results for 
Search instead for 
Did you mean: 

Motor control news from STMicroelectronics - Jan 2014

Gigi
Senior
Posted on January 23, 2014 at 16:00

http://links.st-microelectronics.mkt5947.com/ctt?kn=25&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

http://links.st-microelectronics.mkt5947.com/ctt?kn=22&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

http://links.st-microelectronics.mkt5947.com/ctt?kn=4&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

ST�s motor control software development kit provides all you need for the development of your motor control application based on the STM32 F0, F1, F2, F4 and now F3 (release v3.4) MCUs. It supports up to two PMSMs using any combination of current reading topologies and speed/position sensors, including sensorless operation. Application development and optimization is facilitated by the PC based MC Workbench software. This GUI sets SDK parameters, real-time access to control variables including their display on a virtual oscilloscope.

http://links.st-microelectronics.mkt5947.com/ctt?kn=25&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

Gigi

#stsw-stm32100-pmsm-foc-sdk
12 REPLIES 12
christianwaldmann9
Associate II
Posted on June 05, 2014 at 15:46

On the home page of STSW-32100 the user manual reports already to Version 4.0 of the SDK. There are mentioned more projects for MDKARM we want to use.

UM1080:

 Quick start guide for STM32F PMSM single/dual FOC SDK V4.0

One is: Installation folder\Project\MDK-ARM\STM32F4xx_Workspace.uvmpw

Where and when can I download the

STSW-32100

FOC SDK Version 4.0? A prerelease is o.k. too.

christianwaldmann9
Associate II
Posted on June 11, 2014 at 11:03

Now the Release note are also updated to 4.0, but the download is still 3.4

 

RN0085:

 STM32 PMSM single/dual FOC SDK Release 4.0

Please update the download target too
Gigi
Senior
Posted on June 11, 2014 at 14:10

This mean that the release is imminent...

Ciao

Gigi

christianwaldmann9
Associate II
Posted on June 12, 2014 at 11:46

Thank you for the answer. Can you define ''imminent'' in days?

If the release is not this week, I have to convert the IAR projects myself to MDK-ARM projects, but the projects already exist, as mentioned in the manuals of 4.0.

Gigi
Senior
Posted on June 12, 2014 at 13:56

The plan is to release it by the end of next week with full support of Keil IDE.

Ciao

JackyCheung
Associate II
Posted on June 12, 2014 at 19:21

About release 4.0.0

• Drive Management

– Added HFI sensor less management

– Improved Start-up parameters (start-up rump plotting).

– Added AC Input selection

• Power Stage

– Improved Driving Signals Polarity: Added the possibility to force the same values

for all U, V, W drivers simultaneously.

• Program features:

– Adding Compact/Extend mode: showing/hiding advanced feature.

• Minor bug fixes

waiting

......
christianwaldmann9
Associate II
Posted on June 23, 2014 at 15:06

Hello Gigi

The ''end of next Week'' is over. Do you already have a link to the release. In the online store there is still the Version 3.4.

christianwaldmann9
Associate II
Posted on June 26, 2014 at 16:47

FOC SDK

STSW-STM32100 

Version 4.0.0 is out!

hassanbhutta91
Associate II
Posted on December 04, 2014 at 21:41

hye, Gigi sir i m trying to download 

 PMSM FOC V3.3 firmware ,

but every time my order is rejected, .. kindly help me...