cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 I2C slave

brazov22
Associate II
Posted on October 27, 2011 at 10:18

Hi,

I configured STM32 I2C as slave. I have a master which read data of a valid STM32 I2C register address and then data of an STM32 I2C not valid register address, which is the data expected on the SDA line? After read access on the valid STM32 I2C register address, the STM32 I2C register address is automatically incremented as specified by the protocol?

thanks

brazov
1 REPLY 1
emalund
Associate III
Posted on October 27, 2011 at 15:44

you do not asy if 1xx  or 2xx

if 1xx have you read the errata?

Erik