cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 with Ethernet and FSMC?

ams2
Associate II
Posted on February 23, 2010 at 18:14

STM32 with Ethernet and FSMC?

1 REPLY 1
gahelton1
Associate III
Posted on May 17, 2011 at 13:41

Is ST still woking on the new STM32 with 90nm?

  YES.

Will it have FSMC and Ethernet?  It would be great if it did.

What will be the CPU speed?  Shrinking the geometry almost always will allow an increase in speed along with more memory. How much faster - we will have to wait and see. I would expect a significant speed increase.

If I were me, I'd be excited !

http://www.eetimes.com/news/latest/showArticle.jhtml?articleID=220700360

http://embeddedsystemnews.com/stmicroelectronics-announces-industry’s-first-devices-featuring-embedded-flash-at-90nm-process-technology-based-on-arm-cortex-m-series.html