2012-03-09 03:29 AM
I have a hid report created using descriptor tool 2.4. The final descriptor size is 289. which appears to be to large (hid not detected). If I cut a few reports out so the size becomes less than 256 it works fine. Is it possible to increase the limit or do I need to do something else to get around this.
I'm using STM32_USB-FS-Device_Lib_V3.3.0 Thank you Michael2012-03-09 05:27 PM
Fix wItemLength field of HID descriptor (in the config descriptor set), as follows
usb_desc.c#define WBVAL(x) (x & 0xFF),((x >> 😎 & 0xFF) // <--- add this definitionconst uint8_t CustomHID_ConfigDescriptor[CUSTOMHID_SIZ_CONFIG_DESC] = { ... ... /******************** Descriptor of Custom HID HID ********************/ /* 18 */ 0x09, /* bLength: HID Descriptor size */ HID_DESCRIPTOR_TYPE, /* bDescriptorType: HID */ 0x10, /* bcdHID: HID Class Spec release number */ 0x01, 0x00, /* bCountryCode: Hardware target country */ 0x01, /* bNumDescriptors: Number of HID class descriptors to follow */ 0x22, /* bDescriptorType */ // modify these two lines// CUSTOMHID_SIZ_REPORT_DESC,/* wItemLength: Total length of Report descriptor */// 0x00, WBVAL( CUSTOMHID_SIZ_REPORT_DESC ), /* wItemLength: Total length of Report descriptor */Tsuneo2012-03-10 09:19 AM
2012-03-10 09:58 AM
> your suggestion is pretty
Thanks, but such a macro is a standard way to fill two-bytes numbers into descriptors. You'll see this way in many USB examples from other resources. If ST team would learn the standard way, you shouldn't be trapped. Tsuneo