cancel
Showing results for 
Search instead for 
Did you mean: 

C file function view in STVD?

will2
Associate II
Posted on March 10, 2010 at 16:10

C file function view in STVD?

3 REPLIES 3
frupi2
Associate II
Posted on May 17, 2011 at 15:07

hi!

did you try proprieties of toolbar and check view? Should be this, there is a symbol explorer button. Hope this is what you are looking for.

Ocnarf

will2
Associate II
Posted on May 17, 2011 at 15:07

Hi,

No, that's not what I'm looking for.  The workspace window in STVD (typically on the left-hand side) shows the structure of the workspace, with an expandable folder called ''Source Files'', another one for ''Include Files'', etc.  What I would like to be able to do is change the view so I can expand a C file to show all functions within it.  Seems like every IDE that I've used in the past has this option, but I don't think STVD does.  Hopefully it will be added in future versions as it is a really handy feature.

will2
Associate II
Posted on May 17, 2011 at 15:07

It was confirmed to me by an ST FAE that this is NOT an option on the current release of STVD (4.1.4).

I asked that they add it to the next release.  Fingers are crossed...