cancel
Showing results for 
Search instead for 
Did you mean: 

Un-symmetrically motor current - Design Problem with L6387e

erturki
Associate
Posted on September 18, 2010 at 01:52

Un-symmetrically motor current - Design Problem with L6387e

1 REPLY 1
bille.stello
Associate II
Posted on May 17, 2011 at 10:20

Hello ierturk,

I don't know wether this is the reason of your problem, but from the scheme it looks like the boot capacitor is only 100pF which seemes to me to be a little bit low (consider that it musut keep the charge for two consecutive electrical steps).

Can you try with 100nF (or even more up to 1uF)?

May I ask you whether it is a sensored or sensor-less application?

Regards,

Billino