2018-03-16 08:56 AM
Hi folks,
I am a little confused by the AF selection on some pins in the case of using multiple I2C's.
I am bringing up a new board where board I2C1 and I2C2 are being used on an F4 micro.I2C1 is on PB6 & PB7, I2C2 is on PB9 & PB10.Looking at the MCU manual, it shows for the GPIO AF multiplexer: 'AF4 (I2C1..3, I2CFMP1)'
If I set PB9 to AF4, how is there a distinction between the pin functioning for I2C1 or I2C2?
#i2c #gpio #f42018-03-16 03:40 PM
2018-03-16 07:00 PM
The pin routing on individual pins is clearly shown in the Data Sheet tables. AF Mux on the pin is a 16-to-1 routing, I2C1 presumably has NO routing to PB9, where AF4 is connected to an I2C2 SDA node internally.
Each pin has its own MUX, each mux connects to different NODES.
2018-03-16 11:20 PM
,
,
Aha.
,
So my confusion was partly from using an old version of the ST libraries, which ,has a section of the gpio header with:♯ define
GPIO_AF_I2C1
((
uint8_t
)
0x04
)
/* I2C1 Alternate Function mapping */
♯ define
GPIO_AF_I2C2
((
uint8_t
)
0x04
)
/* I2C2 Alternate Function mapping */
♯ define
GPIO_AF_I2C3
((
uint8_t
)
0x04
)
/* I2C3 Alternate Function mapping */
That confused me, so looking at the manual, I saw that indeed AF4 was allocated for I2C1..3. But what I missed was that AF9 is also a candidate for I2C1..3 connections.
Now that I look into the actual pin function matrix in the device datasheet per your recommendation, I do see that for PB9, AF4 = I2C1_SDA, but AF9 = I2C2_SDA , for PB9.
,
Which led me to check further in st32f4xx_gpio.h, and sure enough, it has:♯ define
GPIO_AF9_I2C2
((
uint8_t
)
0x09
)
/* I2C2 Alternate Function mapping (Only for STM32F401xx/STM32F410xx/STM32F411xE/STM32F412xG/STM32F413_423xx Devices) */
♯ define
GPIO_AF9_I2C3
((
uint8_t
)
0x09
)
/* I2C3 Alternate Function mapping (Only for STM32F401xx/STM32F411xE/STM32F412xG and STM32F413_423xx Devices) */
So I just had to be cognizant of heterogenous ,mappings for the pin muxes, and make the right choices for my project using the old ST libraries.
,
Generating a minimum working example using CubeMX, it does correctly select the pin-specific AF value:GPIO_InitStruct.
Alternate
=
GPIO_AF9_I2C2,
I swear, 'It was right there in the damn datasheet' is going to be the quote on my tombstone ... ,
2018-03-16 11:23 PM
Thanks for the diagram. I don't think this exactly captured the point I was confused about, but nearly: if there was a wire from the I2C2_SDA node up to AF9 of PB9, that would reveal what I was missing.
2018-03-17 03:02 AM
if there was a wire from the I2C2_SDA node up to AF9 of PB9, that would reveal what I was missing.
Should you tell us the particular mcu model you had on your mind, I would have probably guessed what's the source of your confusion and I'd put that wire there.
'an F4 micro' for me is 'F405/'F407/'F415/'F17, as those were the first in the line, historically, and I am working with them a lot.
The crystal ball has its limitations, at least the cheapo model I am using 😉
JW