2010-12-28 06:15 AM
TIM_encodermode_TI1 - why doesnot it count ?
#encoder #timer2011-05-17 05:19 AM
Hi mehmet,
Is the RCC and GPIO well configured for TIM4 ? Can you give us your configuration so perhaps I can help you.Herzlich,MCU Lüfter
2011-05-17 05:19 AM
Hi mehmet,
Your config looks fine. Check that the encoder interface signals are toggling and well connected to PB6 and PB7. Good luck.Herzlich,MCU Lüfter
2011-05-17 05:19 AM
hello thank you , here are the routines I wrote
--------------------------- void TIM4init(void) { TIM_TimeBaseStructure.TIM_Period = 0xffff; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
TIM_EncoderInterfaceConfig(TIM4,TIM_EncoderMode_TI1,TIM_ICPolarity_Rising,TIM_ICPolarity_Rising );
TIM_Cmd(TIM4, ENABLE);
TIM4->CNT=0; } ------------------------------ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9|GPIO_Pin_8|GPIO_Pin_7| GPIO_Pin_6|GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStructure); ------------------------------ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); ------------------------------ and in the main loop { int16_t *RAMptr=&RAM[DATAWORDS+500*2]; *RAMptr= TIM4->CNT; } I can watch the *RAMptr in the PC with my comunication program, no problem there I tried to give pulse PB6 , direction PB7 and vice versa - no counting ( they are TIM4_CH1 & CH2 ) ( btw I have STM32F103RC )2011-05-17 05:19 AM
Hello MCU Lüfter , I think I discovered a bug in STM32 🙂
I checked the signals, everything is fine with my circuit the problem is no matter what encoder mode is selected the Timer counts only phase shifted A B encoder mode I mean I selected TIM_EncoderMode_TI1 and TIM_EncoderMode_TI2 the timer counted only when I simulated phase shifted A B signals on the CH1 and CH2 inputs