cancel
Showing results for 
Search instead for 
Did you mean: 

Graqphics Object/Touch Screen library AN3128

ranjeet_malhotra2
Associate
Posted on June 29, 2010 at 19:35

Graqphics Object/Touch Screen library AN3128

3 REPLIES 3
swhite2
Associate III
Posted on May 17, 2011 at 13:56

I have no idea where to find the source code but like you I'd like to get it.

I did however find the page where AN3128 is referenced from

http://www.st.com/stonline/products/literature/ds/14489/stmpe811.htm

swhite2
Associate III
Posted on May 17, 2011 at 13:56

I have, through my local ST FAE, obtained the source code referenced in AN3128 and have it working on an ST3210E-EVAL board 🙂 It comes with projects for the STM3210B-EVAL, STM3210E-EVAL  and STM3210C-EVAL boards both for IAR's EWARM5 and RealView (RVMDK) v3.50+ toolchains.

I got it in a password-protected ZIP file named

STM3210C-EVAL_TS_Demo_HomePanel with Lib_3.1.2.zip

off an ST support FTP site.

From that I assume that the source in NOT public and is only provided to those that request it.

jgpeiro
Associate
Posted on May 17, 2011 at 13:56

Hi, 

I work on a project with STM32 cpu. I need a graphic library with widgets such as described on AN3128. Can you send me a STM3210C-EVAL_TS_Demo_HomePanel with Lib_3.1.2.zip?

My email addres is _______ at gmail dot com

thanks