cancel
Showing results for 
Search instead for 
Did you mean: 

PWM TIM8_CH2 PC7 Not Working (50%)

kzawada
Associate II
Posted on November 05, 2010 at 21:29

PWM TIM8_CH2 PC7 Not Working (50%)

5 REPLIES 5
Posted on May 17, 2011 at 14:14

I think this for TIM4 is workable, haven't tried TIM8

      /* Time base configuration */

      TIM_TimeBaseStructure.TIM_Period = i16uPeriod - 1; // 0 - (Period - 1) = Period

      TIM_TimeBaseStructure.TIM_Prescaler = i16uPrescalerValue; // Already -1 applied

      TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;

      TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

      TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);

 

      /* PWM1 Mode configuration: Channel2 - 50% */

      TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

      TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

      TIM_OCInitStructure.TIM_Pulse = i16uPeriod / 2; // 50%

      TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;    

      TIM_OC2Init(TIM4, &TIM_OCInitStructure);

      TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable);

 

      TIM_OC2Init(TIM4, &TIM_OCInitStructure);

    

      TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable);

    

      TIM_ARRPreloadConfig(TIM4, ENABLE);

      /* TIM4 enable counter */

      TIM_Cmd(TIM4, ENABLE);

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
kzawada
Associate II
Posted on May 17, 2011 at 14:14

It looks like the counter and the reloading is working just great from the Keil uVision tools.  However, it looks like TIM8_CH2 is not connected to the actual pin (PC7).

How could I trace if the pin (PC7) is getting connected to TIM8_CH2.  I can see that if I use PC7 as standard GPIO output pin I can toggle it easily.   For some reason the mapping that connects TIM8_CH2 to PC7 is missing.  I don't see anything obvious, but it might seem to be something in AFIO.  I have already enabled the AFIO clock.

The register values are the following:

0690X00000604tvQAA.png

Posted on May 17, 2011 at 14:14

I don't have a high density part, I'd be half temped to remap TIM3 on to PC7 and try that. TIM8 should connect right up on your part as best I can tell from here.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
sonhai26988
Associate II
Posted on May 17, 2011 at 14:14

Can you help me?

The Timer 8 is not running. the TIM8_CNT not count...

[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/Timer 8 not working STM32103RD&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%2520CortexM3%2520STM32/AllItems.aspx&currentviews=33]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fTimer%208%20not%20working%20STM32103RD&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FARM%2520CortexM3%2520STM32%2FAllItems%2Easpx&currentviews=33

kzawada
Associate II
Posted on May 17, 2011 at 14:14

Needed to add the following line to connect TIM8_CH2 to PC7:

TIM_CtrlPWMOutputs(TIM8, ENABLE);